Explore the Microchip PIC18 Explorer Board Available from Mouser Electronics
May 28, 2014 - Mouser Electronics, Inc. is now shipping the PIC18 Microcontroller Explorer Board from Microchip Technology. This low cost development kit supports multiple analog and digital inputs, and includes LED indicators and a high resolution 16x2 LCD display. These features allow developers to quickly evaluate the PIC18 microcontroller and prototype projects based on this device.
The Microchip® PIC18 Explorer Board available from Mouser Electronics is a fully featured evaluation and development kit for the board‑mounted 40MHz PIC18F8722 8-bit microcontroller (MCU) with 128KBytes of Flash, 3.9k of RAM, 1KBytes of EEPROM and a 10-bit ADC. The board also comes with a Microchip Plug-In Module (PIM) that has an alternate microcontroller, the high performance 48MHz PIC18F87J11. On-board resources include a 10 kΩ potentiometer for the MCU's analog inputs, eight surface mount LED indicators, an analog temperature sensor, and more. A 16 character by two lines alphanumeric LCD display can be used to provide useful information on the status of the PIC18. All analog and digital pinouts on the PIC18 microcontroller are available for input and output on the header pins.
The PIC18 is Microchip's low power, high end 8-bit microcontroller. The core is extremely efficient and includes a single‑cycle 8x8 hardware multiply. Operating voltage range is from 2.0V to 3.6V and has a sleep current of only 20nA, one of the lowest sleep currents in the industry. With plenty of Flash and ROM, four serial ports and five timers, the PIC18F8722 is ideal for TCP/IP enabled embedded systems, as well as instrumentation panels, industrial control, and smart meters.
Sample programs are provided to demonstrate all the on-chip analog and digital features of the PIC18 microcontrollers, along with all necessary hardware.
To learn more about this PIC18 Explorer Board and read the User's Guide, visit:
http://www.mouser.com/new/microchip/microchip_pic18_explorer/.
With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 20 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser Electronics
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 500 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 400,000 customers in 170 countries from its 492,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About Microchip Technology
Microchip Technology Inc. is a leading manufacturer of microcontroller and analog products, providing low-risk product development, lower total system cost, and faster time to market for thousands of diverse customer applications worldwide. Microchip offers outstanding technical support along with dependable delivery and quality.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Vice President Technical Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Media Communications Manager
(817) 804-7764
Kelly.DeGarmo@mouser.com