Maxim MAX4002x High-Speed Comparators, Now at Mouser, Offer Fast Propagation Delay for LIDAR and ToF Applications
August 8, 2019 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking MAX4002x comparators from Maxim Integrated. Among the fastest low-voltage differential signaling (LVDS) comparators on the market, the MAX40025 and MAX40026 single-supply, high-speed comparators deliver fast propagation delay for distance sensing, time-of-flight (ToF), and high-speed test and measurement instruments.
The Maxim MAX4002x devices, available from Mouser Electronics, are single-supply, high-speed comparators with a typical propagation delay of 280 ps and an extremely low overdrive dispersion of 25ps (typical). The devices are compatible with the outputs of several widely used high-speed transimpedance amplifiers, such as the MAX40658, due to their input common-mode range of 1.5 V to VDD+0.1 V. Both the MAX40025 and MAX40026 run from a supply voltage of 2.7 V to 3.6 V.
The MAX4002x devices can also flexibly interface with many modern FPGAs and CPUs since the devices' output stage is specified for LVDS. This capability enables the comparators to help minimize power dissipation (which aids in system optimization), and complementary outputs help in the suppression of common-mode noise on each output line. Compared to single-ended outputs, the devices' fully differential LVDS outputs deliver the high-speed digital signaling and reduced EMI necessary for a variety of low-noise, high-performance designs.
Maxim's MAX4002x comparators are available in a space-saving, compact 1.218 mm × 0.818 mm WLP package (MAX40025) or an AEC-Q100 automotive-qualified 2 mm × 2 mm TDFN package (MAX40026). For development, Mouser is also stocking the MAX40025EVKIT evaluation kit with layout options that allow engineers to easily modify the input termination.
The MAX4002x comparators are ideal for a broad range of applications, including LIDAR, radar, and sonar; ToF sensors; high-speed differential line receivers; high-speed triggering in oscilloscopes; and communications equipment.
To learn more, visit www.mouser.com/maxim-max4002x-comparators.
With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from nearly 800 manufacturers. Mouser offers 26 support locations around the world to provide best-in-class customer service and ships globally to over 630,000 customers in more than 223 countries/territories from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About Maxim Integrated
Maxim is the leader in analog integration. From mobile to industrial solutions, Maxim is making analog smaller, smarter and more energy efficient.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com